Grundfos CRN pump secures trouble-free operation at the world’s largest producer of viscose staple fibres

Overview_TEXT

Resumen

PT Indo-Bharat Rayon in Puwakarta, Indonesia, is the world’s largest producer of viscose staple fibres. The production is totally dependent on continuous trouble-free operation of steam boilers, generating steam at high temperatures and a maximum pressure of 16 bar.

The system previously operated with a single stage centrifugal pump, but this was found not to meet the company’s very strict demands for reliability and long service intervals.


The situation
PT Indo-Bharat Rayon produces viscose (rayon) staple fibres for the textile industry. The company employs more than 1,000 people and has an annual turnover in excess of USD 122 million. This makes Indo-Bharat Rayon the world’s largest producer of such fibres.

The production is totally dependent on the continuous operation of one steam boiler. The boiler is fitted with an economizer where the boiler flue gas (at 168-276°C) passes over the boiler feed water (at 135°C), thus causing the boiler feed water temperature to increase. This reduces the required energy input with the same rated output and, thus, the boiler efficiency, while reducing operating costs, maintenance costs, water consumption, corrosion in economizer and emissions from the boiler.


The Grundfos solution
The previous solution with a single stage centrifugal pump was found to be unsuitable for the situation, and after careful studies of the extreme operating condition, Grundfos suggested a solution with one CRN 64-2 pump with Air-Cooled Top. This model is suitable for handling liquids at temperatures of up to 180°C. The Grundfos CRN 64-2 offers low NPSH (Net Positive Suction Head) and is well suited for continuous operation under such extreme conditions.

The high efficiency of the CRN model – up to 80 % – results in extremely low energy consumption and low long-term operating costs.


The outcome
Prior to installing the Grundfos CRN range, the Indo-Bharat boiler was subject to frequent unscheduled stops and high maintenance costs. These problems have practically been eliminated, and the pump has been in operation for more than two years, non-stop, and the service or maintenance costs, consequently, have been zero.

The Grundfos CRN pump has completely solved the problems previously encountered, and the savings generated – both in terms of energy consumption and the non-existing service costs – have already more than paid for the pump.

The general outcome has been a much more profitable operation.

Tema:

Reliable, trouble-free operation - No downtime - Reduced service and maintenance costs

Ubicación:

Puwakarta, Indonesia

Empresa:

PT Indo-Bharat Rayon

Grundfos provided

  • Reliable, trouble-free operation
  • No downtime
  • Reduced service and maintenance costs

 

Pumps used

  • Grundfos CRN 64-2 model with Air-Cooled Top.

 

CRN
CRN
Mr. Ajay Shukla
Mr. Ajay Shukla, Power Plant Manager at Indo-Bharat Rayon

“We chose the Grundfos CRN pump because it’s very rare to find a pump that is able to work for such a long time under the very extreme and severe conditions encountered here. The pump has provided excellent service in the last two years’ of 24-hour non-stop operation. There has been no break-downs and the pump has worked during this period with practically zero maintenance.”

Contacts_TEXT

Contacto

Si necesita una solución parecida, por favor, póngase en contacto con nosotros.

Teléfono

918488800

Fax

916280465

Dirección

Camino de la Fuentecilla, s/n
E-28110 Algete (Madrid)

Contacto

Si necesita una solución parecida, por favor, póngase en contacto con nosotros.

Teléfono

918488800

Fax

916280465

Dirección

Camino de la Fuentecilla, s/n
E-28110 Algete (Madrid)