Grundfos helps an innovative Australian water utility

Overview_TEXT

Resumen

Grundfos helps an innovative Australian water utility

The Situation
The Gippsland Water Factory is a wastewater treatment and water-recycling scheme that is being implemented in Maryvale, in the Gippsland region of Victoria.

Fully developed, the multi-stage scheme will treat up to 35 million litres per day of domestic and industrial wastewater, eight million litres of which will be recycled for use by local industry.

Construction of the $130 million dollar project started in 2007 and commissioning is scheduled for 2009.

The Gippsland Water Factory will be the first of its kind in Australia, and the wastewater treatment processes will be ground breaking technology.

Wastewater will be reclaimed using biological treatment followed by microfiltration and reverse osmosis. The Gippsland Water Factory is expected to result in numerous benefits, and will make a significant contribution to the restoration of Gippsland’s waterways and the conservation of its lakes.

The Grundfos Solution
In determining the implementation of Stage One of the Factory, advice was sought from Grundfos.

Gippsland Water Factory wanted to treat up to 35 megalitres of sewage and wastewater per day, including water from the nearby Australian Paper Mills and a tannery.

Following exhaustive investigations and research, Grundfos provided a combination of right mix pumps to Gippsland Water Factory. These included:

  • Grundfos Hydro MPC-E Booster Packages
  • Submersible SEN, SEV, SRP, S1, S2, S3, SEG, EF and Unilift AP Pumps
  • Grundfos PACO Axially Split Case and SS End Suction Pumps
  • Grundfos NKG End Suction Pumps
  • Grundfos WTE Ejectors 
  • Grundfos Chemical Dosing Packages


The Outcome
In Stage One, 32 megalitres of raw sewage is treated through reverse osmosis using bacterial treatment and filtration. 

Eight megalitres of water is treated to an extra high standard and recycled to Australian Paper, which purchases the water. By selling recycled water to Australian Paper, Gippsland Water Factory will save about three billion litres of fresh water in the Moondarra/Latrobe system each year for use in Gippsland.

The remaining 24 megalitres of treated wastewater is sent down the regional outfall sewer (ROS), free of odour causing organics. Removing raw sewage from the ROS and significantly reducing odour in the open channel section is the key driver of Gippsland Water Factory.

The overall result is a savings of about three billion litres of freshwater a year (the equivalent of 1,200 Olympic swimming pools) - be it for environmental flows in rivers, drinking, or to support further growth in the area.

And Grundfos is delighted to have been a part of its exciting Australian “first”.

Tema:

Wastewater treatment

Ubicación:

Victoria, Australia

Empresa:

The Gippsland Water Factory

Contacts_TEXT

Contacto

Si necesita una solución parecida, por favor, póngase en contacto con nosotros.

Teléfono

918488800

Fax

916280465

Dirección

Camino de la Fuentecilla, s/n
E-28110 Algete (Madrid)

Contacto

Si necesita una solución parecida, por favor, póngase en contacto con nosotros.

Teléfono

918488800

Fax

916280465

Dirección

Camino de la Fuentecilla, s/n
E-28110 Algete (Madrid)