Buscar obras de referencia

Mostrar resultados 1 del 10 al 52
Case banner
Ahorros y optimización energética en la estación de bombeo de Mortorum
Propuesta de optimización energética del bombeo de Mortorum desarrollada por Facsa, empresa responsable de la instalación, y consistente en la sustitución de una de las antiguas bombas horizontales existentes por un nuevo grupo de Grundfos, con un rendimiento mucho mayor.
Always the preferred supplier
Lucerne-based milk processor Emmi is the leading Swiss company for cheese and fresh products. Innovations, gains in market share and acquisitions have contributed to several years of sustained growth both in Switzerland and in international markets.
Banking on Hungary
Optimal Hungária is the Hungarian branch of Optimal – a french company that specialises in equipment installation and facility management. Based on previous good experience with Grundfos, the managing director of Optimal regarded Grundfos as the preferred supplier of equipment for a new office block that would serve as the headquarters of ING Bank Hungary, in Budapest.
BM booster - added value for RO plant
OSMOTEC Engineering GmbH, Germany, designs and constructs state-of-the-art Reverse Osmosis, (RO), plants for the purpose of extracting clean drinking water from saline seawater in both offshore and onshore desalination installations.
Bürener Maschinenfabrik GmbH
Bürener Maschinenfabrik GmbH
Charmilles Geneva
Charmilles Geneva
Conserving Bahrain's water resources with Grundfos
Large-scale wastewater pumps from Grundfos help Bahrain conserve its water resources as efficiently as possible.
Control y automatización total
La Central Eléctrica BOT Elektrownia Opole S.A. se encuentra a 9 km de la ciudad de Opole, en el rio Mala Panew que fluye al rio Odra. Las instalaciones de producción exitentes y previstas cubren 290 hectáreas. Esta ubicación asegura una buena oportunidad de suministrar electricidad al área Suroeste de Olonia, así como la transferencia de energía a otras partes del país y del extranjero.
Cutting the cost of district heating
Göteborg Energi is a wholly owned subsidiary of Göteborg Kommunala Förvaltnings AB in Gothenburg, Sweden. The company provides district heating, cooling, natural gas, energy services, an optical fibre network and an electricity supply network. The Göteborg Energi district heating network extends over a length of 700 km, and provides heating for more than 90% of all the apartment blocks in Gothenburg.